adccommunitymod (AutomationDirect) asked a question.

How much oversized can line reactor be?

Created Date: June 26,2018

Created By: bradzik

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Line reactors for higher rated current have lower inductance. The manufacturer of VFD recommends a 4 %, 390 A line reactor at the input. I wonder if I can use bigger line reactors that I already have which are rated for 620 A and have inductance of 26uH. Their percentage impedance value is not given on the nameplate but I made below calculation: % Impedance = ( 2? x f x I x L ) / U * 100 % = 2.19 % f = 50 Hz, I = 620 A, L = 26uH = 0,026 mH = 0,000026 H, U = 400 / sqrt(3) (U is Line to Neutral Voltage in Europe) So apart from thet they are bigger (for higher current) they also have lower percent impedance. I am afraid that running at a lower current their effective percent impedance would be even smaller which also can be calculated from the above formula. Substituting for I the 390 A VFD rated current I get 1,37 % impedance. Is it bad? Would such line reactor offer less protection to the drive?


  • adccommunitymod (AutomationDirect)

    Created Date: June 26,2018

    Created by: bradzik

    Line reactors for higher rated current have lower inductance. The manufacturer of VFD recommends a 4 %, 390 A line reactor at the input. I wonder if I can use bigger line reactors that I already have which are rated for 620 A and have inductance of 26uH. Their percentage impedance value is not given on the nameplate but I made below calculation:

    % Impedance = ( 2? x f x I x L ) / U * 100 % = 2.19 %

    f = 50 Hz, I = 620 A, L = 26uH = 0,026 mH = 0,000026 H, U = 400 / sqrt(3) (U is Line to Neutral Voltage in Europe)

    So apart from thet they are bigger (for higher current) they also have lower percent impedance. I am afraid that running at a lower current their effective percent impedance would be even smaller which also can be calculated from the above formula. Substituting for I the 390 A VFD rated current I get 1,37 % impedance.

    Is it bad? Would such line reactor offer less protection to the drive?

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: June 27,2018

    Created by: Adisharr

    I would contact the manufacturer of the drive in question. I know an oversized one can cause issues in smaller drives if your transformer is significantly higher capacity than what the drive would normally draw. Most of my experience is with much smaller drives though. I can certainly understand why you might want to use what you already have. I'm sure that size reactor is pretty pricey ;)

    Expand Post