adccommunitymod (AutomationDirect) asked a question.
Created Date: February 07,2018
Created By: Kf2qd
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Using a SereServo SVA-2100. Digital Inputs - The diagrams in the manual are not very clear, and show wiring for sinking inputs. The labels on some of the connections are a bit confusing. The COM+ connection is really Digital Input Common and the Digital Inputs do not use COM-. To use the Digital Inputs as Sourcing Inputs then connect positive 24V to the COM+ connection. When the input is pulled to ground it will register as active. For a sinking input connect COM+ to DC Common/DC- and when the input is pulled high it will register as active.
Created Date: February 07,2018
Created by: Kf2qd
Using a SereServo SVA-2100. Digital Inputs -
The diagrams in the manual are not very clear, and show wiring for sinking inputs. The labels on some of the connections are a bit confusing. The COM+ connection is really Digital Input Common and the Digital Inputs do not use COM-.
To use the Digital Inputs as Sourcing Inputs then connect positive 24V to the COM+ connection. When the input is pulled to ground it will register as active. For a sinking input connect COM+ to DC Common/DC- and when the input is pulled high it will register as active.