adccommunitymod (AutomationDirect) asked a question.

6575 Stepper drive

Created Date: January 06,2016

Created By: Adisharr

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

The drive has a rotary POT for selecting motor and current settings. Are there any specifications for the 0-2 POT settings that are labeled as 'reserved ' in the manual?


  • adccommunitymod (AutomationDirect)

    Created Date: January 07,2016

    Created by: Tinker

    Google says:

    "spec·i·fi·ca·tion

    /?spes?f??k?SH(?)n/

    noun

    noun: specification; plural noun: specifications

    an act of describing or identifying something precisely or of stating a precise requirement. "

    Well, while I can understand someone arguing with "precise ", one could make the case that "reserved " IS the specification for settings 0-2, seriously.

    Since it must be cheaper to buy an off the shelf 16 position switch than to have a custom 13 position one made, it is very likely those positions do nothing, and are not a secret mode only special people get to know about.

    If you have a 'scope and a current probe you could experiment, I'd be shocked if any of those settings damaged the drive.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: January 07,2016

    Created by: kewakl

    Since we already have 'tongue planted firmly in cheek, ' ...

    I'd be shocked if any of those settings damaged the drive. ...

    so might the drive..:p

  • adccommunitymod (AutomationDirect)

    Created Date: January 07,2016

    Created by: Adisharr

    hehe I 've actually tried all the settings and they seem to have lower current values than the 'allowable ' settings anyway. I'll probably just check with a voltage / current probe like Tinker suggested.

  • adccommunitymod (AutomationDirect)

    Created Date: January 06,2016

    Created by: Adisharr

    The drive has a rotary POT for selecting motor and current settings. Are there any specifications for the 0-2 POT settings that are labeled as 'reserved ' in the manual?