adccommunitymod (AutomationDirect) asked a question.

Sure Servo - position mode w/analog velocity input

Created Date: October 16,2013

Created By: dumpsta

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I was wondering if theres a way to have this on position mode with analog velocity input. I was looking at the parameters p1.01 and it has a Pt-V dual mode. But in the manual, it says that in position mode, this analog input only controls the max speed, while in velocity mode, the analog input control actual speed. Nothing really about dual mode. My other option is just to set up several positions settings with varying velocities. The sure servo model is the 400watt model Thanks for your help


  • adccommunitymod (AutomationDirect)

    Created Date: December 11,2013

    Created by: oslinjam

    I would like you to help me out with some of the stuff : '(

  • adccommunitymod (AutomationDirect)

    Created Date: December 14,2013

    Created by: LWgreys

    Read the section in Chapter 5 - Dual Control Modes Selection. It has more details on this.

  • adccommunitymod (AutomationDirect)

    Created Date: October 16,2013

    Created by: dumpsta

    I was wondering if theres a way to have this on position mode with analog velocity input.

    I was looking at the parameters p1.01 and it has a Pt-V dual mode.

    But in the manual, it says that in position mode, this analog input only controls the max speed, while in velocity mode, the analog input control actual speed. Nothing really about dual mode.

    My other option is just to set up several positions settings with varying velocities.

    The sure servo model is the 400watt model

    Thanks for your help

    Expand Post