adccommunitymod (AutomationDirect) asked a question.
Created Date: January 14,2013
Created By: perryjenkins
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I have an STP-DRV-4850 that I have been trying to program that seems a little buggy. (It "faults-out " if power is not applied to the high voltage stepper power input first, then a slight delay must be used before applying the 5volt power) At one point the "surestep pro " software told me I needed to update the firmware. (It has older firmware 1.01r ) However I have not been able to locate the update software or firmware binaries. Anyone know if this can be done?
Created Date: January 15,2013
Created by: Do-more PE
There is no firmware update tool available for the SureStep software.
I would suggest that you call in about your 4850 and talk to one of the techs. They may be able to help you determine why this is happening.
Created Date: January 15,2013
Created by: Bdm
Where are you applying 5 Vdc? The 5 vdc on the terminal strip is an output voltage and not an input.
Created Date: January 14,2013
Created by: perryjenkins
I have an STP-DRV-4850 that I have been trying to program that seems a little buggy. (It "faults-out " if power is not applied to the high voltage stepper power input first, then a slight delay must be used before applying the 5volt power)
At one point the "surestep pro " software told me I needed to update the firmware. (It has older firmware 1.01r ) However I have not been able to locate the update software or firmware binaries. Anyone know if this can be done?