adccommunitymod (AutomationDirect) asked a question.
Single phase VFD
Created Date: March 06,2009
Created By: grakkin
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I have an application where I have a 10HP well pump that we want to control with a VFD. The issue is that we only have 230V single phase available at the location. I have heard that you can derate a 3 phase VFD to accept single phase input. I was wondering if the Durapulse line has this functionality and if so are there any drawings available on how to wire the drive with single phase power?
Created Date: March 06,2009
Created by: Do-more PE
All of our drives that can handle a 10HP motor are three phase drives.
Created Date: March 10,2009
Created by: jonesjeremya
Try a STATIC phase converter
If you don't require speed control which is the primary purpose of a VFD, try a phase converter. I would suggest for your application a STATIC phase converter. It will manufacture the third leg, which will be unbalanced (higher voltage) from the two single phase wires. This method should work fine in your application. Static converters can be found on ebay, you can find instructions online how to build one, or you can try this link: http://grizzly.com/products/Static-Phase-Converter-6-to-10-HP/H3473
Good Luck!
Jeremy
Created Date: March 06,2009
Created by: grakkin
I have an application where I have a 10HP well pump that we want to control with a VFD. The issue is that we only have 230V single phase available at the location. I have heard that you can derate a 3 phase VFD to accept single phase input. I was wondering if the Durapulse line has this functionality and if so are there any drawings available on how to wire the drive with single phase power?