adccommunitymod (AutomationDirect) asked a question.

Sure Servo Brake No Brake

Created Date: March 09,2006

Created By: clasentech

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Can someone fill me in on the need for a brake? I thought that if I sent a command to go to position X, that once it got there it would stop and stay there (appropriate decel and all). Is the brake for high speed applications where the windings don't have enough time to responde or is it something else. Thanks


  • adccommunitymod (AutomationDirect)

    Created Date: March 09,2006

    Created by: gkaufman

    This type of brake is a "holding brake ". It is spring-set and released with application of power. In other words, it is acting as a holding brake when power is off. The brake is not intended to stop the servo motor. A holding brake is commonly used in a application where there is a gravity force that might cause the load to move or fall when power is off.

  • adccommunitymod (AutomationDirect)

    Created Date: March 09,2006

    Created by: clasentech

    Ahhh that makes more sense.

    Thanks for the quick reply.

  • adccommunitymod (AutomationDirect)

    Created Date: March 09,2006

    Created by: clasentech

    Can someone fill me in on the need for a brake? I thought that if I sent a command to go to position X, that once it got there it would stop and stay there (appropriate decel and all). Is the brake for high speed applications where the windings don't have enough time to responde or is it something else.

    Thanks