adccommunitymod (AutomationDirect) asked a question.

stepper motor driver

Created Date: March 20,2001

Created By: Aly Gomaa

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I would like to use D4-440 CPU to control a machine, the machine includes three stepper motors (X,Y,A) no encoder is mounted. The HSC module need a driver to drive stepper motor, however the way the machine is build is feedfoward that mean no encoder is connected to check the final position of the stepper motor Can any one suggest a drive to be connected to the HSC to control a 4 wires stepper motor


  • adccommunitymod (AutomationDirect)

    Created Date: March 20,2001

    Created by: Aly Gomaa

    I would like to use D4-440 CPU to control a machine, the machine includes three stepper motors (X,Y,A) no encoder is mounted.

    The HSC module need a driver to drive stepper motor, however the way the machine is build is feedfoward that mean no encoder is connected to check the final position of the stepper motor

    Can any one suggest a drive to be connected to the HSC to control a 4 wires stepper motor

    Expand Post