adccommunitymod (AutomationDirect) asked a question.

D0-06DD1 connecting to PC and HMI

Created Date: October 20,2015

Created By: Biederboat

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Hi, First time working with a D0-06 series (more used to the 05's but still very much a novice overall). The 05's come with two "phone " jack plugs or whatever they are called (RJ45?) for Port1 & 2 serial ports and I use one for a C-more and the other to program with. On the 06, one of the ports is RJ45 and the other is a regular serial connection (DB9?). I have programming cables that use the RJ45 connector, none with the DB9 (and the C-more needs a RJ45). Is my only option, in order to program the PLC without interrupting the connection to the HMI, to get a programming cable with the DB9? I don't even really see an option to purchase such a cable on their website. Any other way to go? I don't even see an option to buy a module with the RJ45 connector. Thanks, BB


  • adccommunitymod (AutomationDirect)

    Created Date: October 20,2015

    Created by: bcarlton

    Use a FA-15HD as an adapter between the 15 pin port and a RJ12 (not RJ45) jack. Then plug your cable into that.

  • adccommunitymod (AutomationDirect)

    Created Date: October 21,2015

    Created by: jackson

    Another option (depending upon your distance between the C-more panel and the PLC) is the EA-2CBL-1. It is designed specifically for that purpose.

    So you can use your existing cable to program the PLC on port 1 and plug the C-more panel into port 2.

  • adccommunitymod (AutomationDirect)

    Created Date: October 21,2015

    Created by: Biederboat

    Thanks guys, appreciate the info!

    BB

  • adccommunitymod (AutomationDirect)

    Created Date: October 20,2015

    Created by: Biederboat

    Hi,

    First time working with a D0-06 series (more used to the 05's but still very much a novice overall). The 05's come with two "phone " jack plugs or whatever they are called (RJ45?) for Port1 & 2 serial ports and I use one for a C-more and the other to program with. On the 06, one of the ports is RJ45 and the other is a regular serial connection (DB9?). I have programming cables that use the RJ45 connector, none with the DB9 (and the C-more needs a RJ45).

    Is my only option, in order to program the PLC without interrupting the connection to the HMI, to get a programming cable with the DB9? I don't even really see an option to purchase such a cable on their website. Any other way to go? I don't even see an option to buy a module with the RJ45 connector.

    Thanks,

    BB

    Expand Post