adccommunitymod (AutomationDirect) asked a question.

DL06 with encoder (very slow pulse, no high speed)

Created Date: March 19,2015

Created By: Langleym

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Has anyone tried using encoders on normal I/O points on that Plc? The application will run a 360 ppm encoder at 3 rpm. That's 1 pulse per 56ms. The scan time and on-off I/o times are much lower, like 4-8ms. If I am thinking correctly it should be fine, my only worry is if the machine stops right on a pulse edge and it flutters I might get phantom pulses. The reason I am asking is because I would like to use the high speed output for a stepper and I need to read this slow encoder and possibly another higher speed one, and my expansion ports are quickly filling up. (Budget minded too)


  • adccommunitymod (AutomationDirect)

    Created Date: March 20,2015

    Created by: 1st.vtbowman

    counter

    Doesn't the 06 allow X0 and X1 to be programmed as high speed counter.

  • adccommunitymod (AutomationDirect)

    Created Date: March 20,2015

    Created by: Langleym

    It allows 1 HSIO, it can be either the input or output but not at the same time i believe.

  • adccommunitymod (AutomationDirect)

    Created Date: March 20,2015

    Created by: ControlsGuy

    That sounds feasible. I 've never done it with an 06, but have with other PLC's with good results.

  • adccommunitymod (AutomationDirect)

    Created Date: March 19,2015

    Created by: Langleym

    Has anyone tried using encoders on normal I/O points on that Plc? The application will run a 360 ppm encoder at 3 rpm. That's 1 pulse per 56ms. The scan time and on-off I/o times are much lower, like 4-8ms.

    If I am thinking correctly it should be fine, my only worry is if the machine stops right on a pulse edge and it flutters I might get phantom pulses.

    The reason I am asking is because I would like to use the high speed output for a stepper and I need to read this slow encoder and possibly another higher speed one, and my expansion ports are quickly filling up. (Budget minded too)

    Expand Post