adccommunitymod (AutomationDirect) asked a question.
Do-more to SureServo ALE19 help
Created Date: December 30,2014
Created By: Gerry G
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I have a Do-more cpu with a h2-serio-4 card, using the svc-232rj12-cbl. I set the h2-serio-4 port A to Modbus RTU Client (master) Settings Baud 19200 Data 8 Stop 1 Parity Odd Same as the drive Any ideas on why I'm getting alarm 19 Thanks
Created Date: December 30,2014
Created by: Gerry G
Well, I got ALE19 alarm cleared up. ended up clearing the drive and starting over not sure what went wrong the first time thru, but it's working now.
On to the next hurtle, if any one out there has a working DO-More program with Modbus to control a SureDrive Servo, for positioning control. I would love to take a look at it. All the manuals are all written for DS5 and half of the instructions do no cross vary well. I have the drive moving around and am able to set speed and position, but it is one of the ugliest programs I 've seen.
Any advice would be great.
Created Date: December 30,2014
Created by: Gerry G
I have a Do-more cpu with a h2-serio-4 card, using the svc-232rj12-cbl.
I set the h2-serio-4 port A to Modbus RTU Client (master)
Settings
Baud 19200
Data 8
Stop 1
Parity Odd
Same as the drive
Any ideas on why I'm getting alarm 19
Thanks