adccommunitymod (AutomationDirect) asked a question.
DL06 Port 2 will not communicate
Created Date: June 16,2014
Created By: david222
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I need to get a program out of a DL06 for validation purposes. I have the cable that connects to Port 2. Can I communicate thru this port or does it have to be Port 1? I have tried auto communication. Thanks
Created Date: June 16,2014
Created by: Bob S BN
Port 1 is the fixed settings programming port.
I believe Port 2 can be used for programming if the port settings are correct to match the programming computer. However, you need the programming software connected or the PLC program logic to change the port 2 settings.
Created Date: June 16,2014
Created by: scott.lawrence
only if it was set-up in software...
Created Date: June 16,2014
Created by: Do-more PE
If you have any communication instructions in the PLC that use Port 2, you will need to put the PLC in STOP mode in order to connect.
Created Date: June 16,2014
Created by: david222
I need to get a program out of a DL06 for validation purposes. I have the cable that connects to Port 2. Can I communicate thru this port or does it have to be Port 1? I have tried auto communication.
Thanks