adccommunitymod (AutomationDirect) asked a question.
Created Date: April 04,2014
Created By: Gunner
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I am trying to read a load cell, and must have something wrong. I have attached a screenshot of the ladder code. I have all of the - inputs tied to ground, the strain gage excitation is independent (9V battery). The other wires from the bridge are connected to ch 1, one to + and one to -. I can see the voltage at the inputs vary from 0.1 mV to 10 mV. The output on the LCD module stay at 10087 for line 1, and 3 for line 2. Would anybody have any ideas on what I am missing?
Created Date: April 04,2014
Created by: Gunner
I am trying to read a load cell, and must have something wrong.
I have attached a screenshot of the ladder code.
I have all of the - inputs tied to ground, the strain gage excitation is independent (9V battery). The other wires from the bridge are connected to ch 1, one to + and one to -.
I can see the voltage at the inputs vary from 0.1 mV to 10 mV.
The output on the LCD module stay at 10087 for line 1, and 3 for line 2.
Would anybody have any ideas on what I am missing?