adccommunitymod (AutomationDirect) asked a question.

Do-More with old backplane?

Created Date: March 27,2014

Created By: bgirouard

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I have some old DL-205 series bases that does not have the expansion port on the end (e.g. D2-04 for a four-slot base). Can this be used with a Do-More, or is it required to use a new base (e.g. D2-06BDC1-1)?


  • adccommunitymod (AutomationDirect)

    Created Date: March 27,2014

    Created by: franji1

    It should work. Do-more does not support EM/CM for expansion anyway. It does support Ethernet I/O on the Ethernet port of the H2-DM1E CPU for up to 16 slaves of I/O, including GSEDrives.

  • adccommunitymod (AutomationDirect)

    Created Date: March 27,2014

    Created by: bgirouard

    I have some old DL-205 series bases that does not have the expansion port on the end (e.g. D2-04 for a four-slot base). Can this be used with a Do-More, or is it required to use a new base (e.g. D2-06BDC1-1)?