adccommunitymod (AutomationDirect) asked a question.

H2-Citrio Raw Counter Value changes?

Created Date: February 11,2013

Created By: ctvowels1

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Is it possible to adjust the Raw value in the H2-Citrio. I have DW Real Value converted to DW BCD. Not Sure there is a method to convert DW BCD or DW Real to Decimal ? Or is it possible to convert to DW Binary and then Load the value to the H2-Citrio via the WT instruction? Frustrating changing a program from DL06 to D260. :mad:


  • adccommunitymod (AutomationDirect)

    Created Date: February 11,2013

    Created by: ctvowels1

    Is it possible to adjust the Raw value in the H2-Citrio.

    I have DW Real Value converted to DW BCD.

    Not Sure there is a method to convert DW BCD or DW Real to Decimal ?

    Or is it possible to convert to DW Binary and then Load the value to the H2-Citrio via the WT instruction?

    Frustrating changing a program from DL06 to D260.

    :mad:

    Expand Post