adccommunitymod (AutomationDirect) asked a question.
Created Date: November 17,2012
Created By: renhoek
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Hello all, I cant seem to connect H2-DM1e to my router Click new connection ethernet in the link wizard Udp/p No mac adress in default adapter but shows up when switched to intel 8256lf-2 IP shows 255.255.255.255 Query blinks Eth led click next error connecting to PLC Ext error: Timeout error netedit shows same data when I switch from default adapter to intel I have tried different computers and different cables. Runing windows 7 Anyone have an idea of what is going on? I have no trouble connecting via USB Thanks, TJ
Created Date: November 17,2012
Created by: franji1
Use NetEdit to assign the DM1E's IP Address along with its subnet mask. You can also do it from within Do-more Designer using the USB link (PLC->System Information, then in the lower middle is the Set Node and IP Configuration button to configure those settings).
Make sure your IP Address and Subnet Mask are consistent with the PC running Designer. Once you have the PLC's IP Address and subnet mask established, then you should be able to create an Ethernet link using the Link Wizard from Designer.
Created Date: November 17,2012
Created by: renhoek
That was it; works now
Thanks
Created Date: November 17,2012
Created by: renhoek
Hello all,
I cant seem to connect H2-DM1e to my router
Click new connection
ethernet in the link wizard
Udp/p
No mac adress in default adapter but shows up when switched to intel 8256lf-2
IP shows 255.255.255.255
Query blinks Eth led
click next
error connecting to PLC
Ext error: Timeout error
netedit shows same data when I switch from default adapter to intel
I have tried different computers and different cables. Runing windows 7
Anyone have an idea of what is going on?
I have no trouble connecting via USB
Thanks,
TJ