adccommunitymod (AutomationDirect) asked a question.
B10000.0?
Created Date: August 27,2012
Created By: flux70
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
DL205 rack CPU: D250 at least. Not really sure just yet. I dont know what this coil address is. Never seen it or used it. It is in a rung with a Y0 in front of it. When Y0 is true, the output coil B10000.0 is activated. When Y0 is not true, B10000.1 is activated. Can someone explain what this address is? I didnt write the program. Just trying to help a friend.
Created Date: August 28,2012
Created by: daakers
Bit of Word bit 0 of word 10000
Created Date: August 28,2012
Created by: Bob S BN
Bit of Word bit 0 of word 10000
To expand on this a bit, Vmemory word V10000 is being broken down into 16(0-15) individual discrete bits.
I 've had to use this feature with some Optimate HMI panels from AD to trigger the button lights and to read the buttons, because that's how they were designed.
Created Date: August 27,2012
Created by: flux70
DL205 rack
CPU: D250 at least. Not really sure just yet.
I dont know what this coil address is. Never seen it or used it. It is in a rung with a Y0 in front of it.
When Y0 is true, the output coil B10000.0 is activated.
When Y0 is not true, B10000.1 is activated.
Can someone explain what this address is? I didnt write the program. Just trying to help a friend.