adccommunitymod (AutomationDirect) asked a question.

voltage problem in IO

Created Date: April 06,2012

Created By: tgmarc86

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I'm using f2-08AD-2 to read a 0 10 V source, I have the jumper for 0-10/0-5 removed as the manual requires to read 0-10. At a 1 Volt reading from the source, I'm getting 900 out of the PLC, which would be correct if it was on the 0-5V setting. If I add the jumper to go to 0-5 I get twice that, which is logical. It's as if I'm missing something in the programming to let it know I'm reading at 0-10 not 0-5. Can anyone help with this dilemma?


  • adccommunitymod (AutomationDirect)

    Created Date: April 06,2012

    Created by: bcarlton

    I'm getting 900 out of the PLC

    This is very vague

    Exactly what instructions are you using see the reading. Be sure that you are using the correct mode for viewing the number.

  • adccommunitymod (AutomationDirect)

    Created Date: April 06,2012

    Created by: tgmarc86

    I'm using f2-08AD-2 to read a 0 10 V source, I have the jumper for 0-10/0-5 removed as the manual requires to read 0-10. At a 1 Volt reading from the source, I'm getting 900 out of the PLC, which would be correct if it was on the 0-5V setting. If I add the jumper to go to 0-5 I get twice that, which is logical. It's as if I'm missing something in the programming to let it know I'm reading at 0-10 not 0-5. Can anyone help with this dilemma?

    Expand Post