adccommunitymod (AutomationDirect) asked a question.
Created Date: March 14,2012
Created By: ricowind
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I have a small project and I am putting together and have acquired a H2-WPLC1 device and had a few questions concerning the use of this device as well as what my needs for this project. I want the end project to have the following capabilities for use on 1 PC • HMI creation with control • Data and trend logging The system is a DL 205, 9 slot devices with 1 expansion module; I would like to add the H2-WPLC1 to access and control from 1 PC • I have been reading that the Demo software that you offer will work with some scenarios but from the request I have above will the demo version work? • I see that you used to offer a Starter kit, but it is discontinued is there something you offer that is for a 1 user 1 PC device and what will it cost? There is quite a bit of documentation on the think and do environment, with my requests of what I would like my system to perform, what will I need to purchase and how much?
Created Date: March 14,2012
Created by: ricowind
I have a small project and I am putting together and have acquired a H2-WPLC1 device and had a few questions concerning the use of this device as well as what my needs for this project.
I want the end project to have the following capabilities for use on 1 PC
• HMI creation with control
• Data and trend logging
The system is a DL 205, 9 slot devices with 1 expansion module; I would like to add the H2-WPLC1 to access and control from 1 PC
• I have been reading that the Demo software that you offer will work with some scenarios but from the request I have above will the demo version work?
• I see that you used to offer a Starter kit, but it is discontinued is there something you offer that is for a 1 user 1 PC device and what will it cost?
There is quite a bit of documentation on the think and do environment, with my requests of what I would like my system to perform, what will I need to purchase and how much?