adccommunitymod (AutomationDirect) asked a question.

Questions concerning Demo software for Look and do with H2-WPLC1 device

Created Date: March 14,2012

Created By: ricowind

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I have a small project and I am putting together and have acquired a H2-WPLC1 device and had a few questions concerning the use of this device as well as what my needs for this project. I want the end project to have the following capabilities for use on 1 PC • HMI creation with control • Data and trend logging The system is a DL 205, 9 slot devices with 1 expansion module; I would like to add the H2-WPLC1 to access and control from 1 PC • I have been reading that the Demo software that you offer will work with some scenarios but from the request I have above will the demo version work? • I see that you used to offer a Starter kit, but it is discontinued is there something you offer that is for a 1 user 1 PC device and what will it cost? There is quite a bit of documentation on the think and do environment, with my requests of what I would like my system to perform, what will I need to purchase and how much?


  • adccommunitymod (AutomationDirect)

    Created Date: March 14,2012

    Created by: ricowind

    I have a small project and I am putting together and have acquired a H2-WPLC1 device and had a few questions concerning the use of this device as well as what my needs for this project.

    I want the end project to have the following capabilities for use on 1 PC

    • HMI creation with control

    • Data and trend logging

    The system is a DL 205, 9 slot devices with 1 expansion module; I would like to add the H2-WPLC1 to access and control from 1 PC

    • I have been reading that the Demo software that you offer will work with some scenarios but from the request I have above will the demo version work?

    • I see that you used to offer a Starter kit, but it is discontinued is there something you offer that is for a 1 user 1 PC device and what will it cost?

    There is quite a bit of documentation on the think and do environment, with my requests of what I would like my system to perform, what will I need to purchase and how much?

    Expand Post