adccommunitymod (AutomationDirect) asked a question.
Created Date: May 26,2011
Created By: sdav99
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I am setting up a DL06 system with a F0-08ADH-1 analog input card (4-20mA current loop). The F0-08ADH-1 analog input card will receive analog output signals from an instrument that can provide 4-20mA against a max 500 ohm load using its analog output card. The shield is not landed at the instrument. Documentation for F0-08ADH-1 shows one lead to Ch1, the shield to COM and the other lead to +24VDC. How should it be wired? One lead to Ch1 and the other and shield to COM?
Created Date: May 27,2011
Created by: Do-more PE
We need more information on the instrument itself to give a satisfactory answer.
Created Date: May 27,2011
Created by: sdav99
Thanks; I'll give tech support a call and discuss the specifics.
Created Date: May 26,2011
Created by: sdav99
I am setting up a DL06 system with a F0-08ADH-1 analog input card (4-20mA current loop). The F0-08ADH-1 analog input card will receive analog output signals from an instrument that can provide 4-20mA against a max 500 ohm load using its analog output card. The shield is not landed at the instrument.
Documentation for F0-08ADH-1 shows one lead to Ch1, the shield to COM and the other lead to +24VDC.
How should it be wired? One lead to Ch1 and the other and shield to COM?