adccommunitymod (AutomationDirect) asked a question.

ASCII Scale Weight to D2-260

Created Date: May 20,2011

Created By: russh

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I have an application, using a D2-260 CPU, where I need to read two weights coming from a dual-channel scale that transmits ASCII continually. Do I use an H2-SERIO?


  • adccommunitymod (AutomationDirect)

    Created Date: May 21,2011

    Created by: bcarlton

    H2-SERIO - SERIAL MODULE, 3 RS-232 PORTS, FOR USE WITH WINPLC & H2-EBC100

    Is the information coming in on two separate serial lines? If so check out the F2-CP128 BASIC module.

  • adccommunitymod (AutomationDirect)

    Created Date: May 24,2011

    Created by: russh

    Yes - the information will come in on two seperate serial lines. I am not familiar with the F2-CP128 but will check it out. Thanks!

  • adccommunitymod (AutomationDirect)

    Created Date: May 24,2011

    Created by: bcarlton

    Using the BASIC module you'll be able to listen to the two lines, receiving the ASCII, do the ASCII -> Numeric conversion and send the converted information directly into the CPU's memory. The BASIC programming is fairly easy.

  • adccommunitymod (AutomationDirect)

    Created Date: May 20,2011

    Created by: russh

    I have an application, using a D2-260 CPU, where I need to read two weights coming from a dual-channel scale that transmits ASCII continually. Do I use an H2-SERIO?