adccommunitymod (AutomationDirect) asked a question.

Battery Replacement D4-405

Created Date: April 06,2011

Created By: PrisonSparky

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Can the D4-BAT in the D4-450 CPU and the D4-MC-BAT in the D4-RAM-2 be "hot swapped " or does the PLC need to be powered off? Thanks in advance.


  • adccommunitymod (AutomationDirect)

    Created Date: April 06,2011

    Created by: Do-more PE

    The D4-BAT can be hot swapped, but there isn't any way to swap the battery in the Memory module without removing it from the PLC.

  • adccommunitymod (AutomationDirect)

    Created Date: April 06,2011

    Created by: PrisonSparky

    Thank you, so obviously removing the memory cartridge would disrupt the program, so a shut down is necessary.

  • adccommunitymod (AutomationDirect)

    Created Date: April 06,2011

    Created by: PrisonSparky

    Can the D4-BAT in the D4-450 CPU and the D4-MC-BAT in the D4-RAM-2 be "hot swapped " or does the PLC need to be powered off?

    Thanks in advance.