adccommunitymod (AutomationDirect) asked a question.

Cable from DL-260 port2 to DL05 port2

Created Date: April 04,2011

Created By: Tubecut

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I need a cable (RJ12) from the FA-15HD used for DL260 port2 to connect to a DL05 port2. I have a cable that is used with the USB adapter EA-MG-PGM-CBL to connect the PC to the DL260 for programming. At one time I thought there was a PDF document that listed all of the AD cables and the configuration/pin outs for each. I think the existing cable used with the EA-MG-PGM-CBL adapter is a DV1000 cable. Can anyone clarify this and also point me in the right direction to a cable pin out diagram(s)? I want to connect the 260 as master and the 05 as slave.


  • adccommunitymod (AutomationDirect)

    Created Date: April 04,2011

    Created by: Tubecut

    Thanks Glenn. That cable diagram is some help. But, what I am actually looking for as a cable (RJ12) that would go from the FA-15HD adapter which is a 15 pin to RJ12 adapter and the RJ12

    cable would then connect to the DL05 port2. This should allow for connect between the DL260 and the DL05.

    At one time , I thought there was a PDF that listed all of the various AD cables. It was just a single PDF file as I recall.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: April 04,2011

    Created by: Tubecut

    I need a cable (RJ12) from the FA-15HD used for DL260 port2 to connect to a DL05 port2.

    I have a cable that is used with the USB adapter EA-MG-PGM-CBL

    to connect the PC to the DL260 for programming. At one time I thought there was a PDF document that listed all of the AD cables

    and the configuration/pin outs for each.

    I think the existing cable used with the EA-MG-PGM-CBL adapter is a DV1000 cable. Can anyone clarify this and also point me in the right direction to a cable pin out diagram(s)?

    I want to connect the 260 as master and the 05 as slave.

    Expand Post