adccommunitymod (AutomationDirect) asked a question.

Initial setup for ECOM, why won't Router work but switch will?

Created Date: December 09,2010

Created By: dieselvette

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Two questions: 1) When the computer & ECOM are both plugged into the LAN side of a router (tried a couple of different routers) I cannot gain access to the ECOM to initially setup the IP (but it works with a switch). Would this be due to a limitation of the router, or what is missing here? I would expect the LAN side of a router to work just like a switch (but with a DHCP server & other capabilities.) 2) Instead of using a switch or router, if I had a crossover cable could I connect directly to the ECOM to set it up? Once I 've put the IP in the ECOM and then set up the router correctly, everything is fine. What I'm trying to get away from is needing a switch temporarily just for initial ECOM setup.


  • adccommunitymod (AutomationDirect)

    Created Date: December 09,2010

    Created by: bcarlton

    The crossover should definately do it.

  • adccommunitymod (AutomationDirect)

    Created Date: January 10,2011

    Created by: dieselvette

    In short, I 've tried different types of routers and tried a crossover cable and had very little success in being able to set up the ECOM with anything other than a simple GS105 switch (with or without being on a DHCP network).

    I don't understand why the crossover cable won't work for initial setup or comm after setup. If the ECOM has it's IP already set, it will respond to a ping over the xover cable (and is fully functional with a router), but will not establish comm with DS5 with a xover cable.

    Could it be a setting on my comp? Our IT person tried a couple of adjustments but we lost patience there pretty fast (because it's non-critical as long as I always have a switch in my back pocket).

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: January 10,2011

    Created by: Shimmy

    I use a crossover cable to setup ecom-100s and it works everytime. Do you have IPX setup on your PC?

  • adccommunitymod (AutomationDirect)

    Created Date: January 11,2011

    Created by: Bob S BN

    I'm no expert at this, only done a couple systems, but I have a thought.

    Because I was dealing with 3 different brands of equipment, each came with it's own factory initial address. I found I had to change the laptop address and subnet(I think that's the term) so they were both in the same neighborhood, then I could connect, change address, and disconnect. Get all equipment and laptop with similar addresses, and then things worked right.

    Just a thought,

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: January 11,2011

    Created by: GKiser

    Two questions:

    1) When the computer & ECOM are both plugged into the LAN side of a router (tried a couple of different routers) I cannot gain access to the ECOM to initially setup the IP (but it works with a switch). Would this be due to a limitation of the router, or what is missing here? I would expect the LAN side of a router to work just like a switch (but with a DHCP server & other capabilities.)

    The reason this doesn't work is because NetEdit uses a broadcast to find the ECOMs on the network. All routers, by default, block broadcasts of any kind.

    2) Instead of using a switch or router, if I had a crossover cable could I connect directly to the ECOM to set it up?

    Crossover should work, unless you have more than one NIC (Network Interface Card) enabled (e.g. a wired, and a wireless). Try disabling the wireless NIC and see if it works.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: January 14,2011

    Created by: bartb102

    Yes, two active network connection cards can often cause a problem. The software usually picks the wrong one.

  • adccommunitymod (AutomationDirect)

    Created Date: December 09,2010

    Created by: dieselvette

    Two questions:

    1) When the computer & ECOM are both plugged into the LAN side of a router (tried a couple of different routers) I cannot gain access to the ECOM to initially setup the IP (but it works with a switch). Would this be due to a limitation of the router, or what is missing here? I would expect the LAN side of a router to work just like a switch (but with a DHCP server & other capabilities.)

    2) Instead of using a switch or router, if I had a crossover cable could I connect directly to the ECOM to set it up?

    Once I 've put the IP in the ECOM and then set up the router correctly, everything is fine. What I'm trying to get away from is needing a switch temporarily just for initial ECOM setup.

    Expand Post