adccommunitymod (AutomationDirect) asked a question.
Created Date: September 01,2010
Created By: brittonc
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Hello Everyone I need help with a PLC that is being used to control a medium sized composite bake oven. This is a urgent project that I need done right way. I have a DL06 equipped with Thermocouple Input cards and a 4 channel 4-20ma Analog Output card. The display and interface is running on a 10 " C-More touch screen. The programmer we were using dissapeared and I am looking for a programmer who can help us finish our program. The basics are all there including the control and user interface. I need to get the PLC to have better control over the ramp up/down of the oven tempature as well as record the entire process and give a print out at the end. If anyone has any intrest in working with us on this please email at britton.coulson@coulsongroup.com . Thanks for your time, Britt
Created Date: September 01,2010
Created by: brittonc
Hello Everyone
I need help with a PLC that is being used to control a medium sized composite bake oven. This is a urgent project that I need done right way.
I have a DL06 equipped with Thermocouple Input cards and a 4 channel 4-20ma Analog Output card. The display and interface is running on a 10 " C-More touch screen.
The programmer we were using dissapeared and I am looking for a programmer who can help us finish our program. The basics are all there including the control and user interface. I need to get the PLC to have better control over the ramp up/down of the oven tempature as well as record the entire process and give a print out at the end.
If anyone has any intrest in working with us on this please email at britton.coulson@coulsongroup.com .
Thanks for your time,
Britt