adccommunitymod (AutomationDirect) asked a question.
dl06 convertions
Created Date: August 14,2010
Created By: rodtech35
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
i am needing to use double word in the ladder program. it shows up in the data view when i switch it to double word but it shows up in ladder program as a zero. is there a way to use double as a greater than or equal to???
Created Date: August 14,2010
Created by: milldrone
rodtech35,
Try this
PLC 06
// Rung 1
// Address 0
STR SP0
LD K400
OUT V700
LDA O2000
OUT V701
// Rung 2
// Address 5
STR SP1
LD K5000
MUL V2000
DIV K4095
MUL K100
OUTD V2030
// Rung 3
// Address 11
STR SP1
TMR T0 K80
// Rung 4
// Address 15
STR SP4
AND T0
OUT C100
// Rung 5
// Address 18
STR C100
STR CT0
CNT CT0 V2060
// Rung 6
// Address 22
STRE CTA0 V2061
OUT C102
// Rung 7
// Address 25
#BEGIN COMMENT
"Making a presumption that V3000 is a double word also. If it is not a double word then "
"V3001 must contain zero "
" "
"You must use the SP61 SP62 or SP63 special relays before another function uses them "
#END
STR SP1
LDD V2030
CMPD V3000
STR SP62
OR SP61
ANDSTR
OUT C41
// Rung 8
// Address 32
#BEGIN COMMENT
"You can also do a LDF (load formatted) and a OUTF (out formatted) to save the bits for "
"use later in the logic if needed. In this case SP60, SP61, SP63, are saved to C1000, "
"C1001, C1002 "
#END
STR SP1
LDF SP60 K3
OUTF C1000 K3
// Rung 9
// Address 37
END
// Rung 10
// Address 38
STR V2030 V3000
OUT C41
// Rung 11
// Address 41
END
// Rung 12
// Address 42
NOP
#BEGIN ELEMENT_DOC
"C41 ", " ", " ", "HIGH SAND LEVEL "
"C1000 ", " ", " ", "less than the instruction value SAVED "
"C1001 ", " ", " ", "equal to the instruction value SAVED "
"C1002 ", " ", " ", "greater than the instruction value SAVED "
"V2030 ", " ", " ", "SCALED LEVEL "
"V3000 ", " ", " ", "sand alarm "
"SP60 ", " ", " ", "less than the instruction value "
"SP61 ", " ", " ", "equal to the instruction value "
"SP62 ", " ", " ", "greater than the instruction value "
#END
Created Date: August 14,2010
Created by: rodtech35
Thank you very much is there somewhere in the manual it explain how you came up with that???? just wondering for future project. never had to scale this high before.:eek: By the way v3000 was double also
Created Date: August 14,2010
Created by: milldrone
is there somewhere in the manual it explain how you came up with that?
Page 5-82, an index for the functions is on page 5-2, 5-3, and 5-4. I paid for the hardcopy version of the manual and those three pages are very dirty and dogeared.
Created Date: August 14,2010
Created by: rodtech35
i am needing to use double word in the ladder program. it shows up in the data view when i switch it to double word but it shows up in ladder program as a zero. is there a way to use double as a greater than or equal to???