adccommunitymod (AutomationDirect) asked a question.

DL260 Port 1 RS-232 communication

Created Date: May 04,2010

Created By: timjan2005

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I am new to Direct Logic 205. I am programming with DirectSOFT 5. I am trying to communicate through PORT 1 of my DL260 using RS-232 to a rice lake wieght scale indicator. I have serched for code examples and the help files for examples but can not find any examples showing exactly how to write my program code where i can read the serial information coming in from the rice lake. I appreciate any help. thanks Tim


  • adccommunitymod (AutomationDirect)

    Created Date: May 04,2010

    Created by: bcarlton

    Download the manual for the DL-260 from AutomationDirect and read about the capabilities of the ports.

  • adccommunitymod (AutomationDirect)

    Created Date: May 04,2010

    Created by: timjan2005

    Thanks PLC guy. I 've looked/read the manual for some time now. I can not find any code examples which is my main reason for the post. If i'm over looking code examples in the port capabilities section please be more specific to what page.

  • adccommunitymod (AutomationDirect)

    Created Date: May 04,2010

    Created by: bcarlton

    You will probably be implementing an ASCII interface. That is not available through Port 1. One way - usually receive only - ASCII operation is available on Port 2. It is not really set up for two way ASCII messages. Also check out possible examples in the Application Notes

    You will have to use transmission information from Rice Lake. Read the information in the PLC manual regarding ASCII communication. Then start writing your own code using the minimal example under the AIN instruction.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: May 04,2010

    Created by: timjan2005

    I am wanting to use the RS-232 on port 1. The indicator i'm trying to talk to is RS-232 9600 baud 8bitt odd parity with 1 stop bit, 1 start bit.

  • adccommunitymod (AutomationDirect)

    Created Date: May 04,2010

    Created by: bcarlton

    Communication is more than just electrical and speed compatibility. What protocol is the weigher using? See if that is compatible with Port 1.

  • adccommunitymod (AutomationDirect)

    Created Date: May 04,2010

    Created by: timjan2005

    ok that was a good question. i guess i just assumed rs-232 didn't have a "protocol " other than the settings had to be the same. But i did read that my indicator will only except ASCII.

    "...serial commands can be sent using any external device capable of sending ASCII characters over a serial connection... "

    I know my PORT 1 won't do ASCII.

    I already have planes for PORT 2 on my DL260. So maybe i need to look into buying the ethernet expansion board on my indicator and talk to if through the H2-ECOM100.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: May 04,2010

    Created by: bcarlton

    Just because you may make a connection with an Ethernet cable don't think you don't have to match protocols also.

  • adccommunitymod (AutomationDirect)

    Created Date: May 04,2010

    Created by: KPrice

    timjan2005, Since your DL260 Port 2 is taken, an option is the CoProc module for the 205. The CoProc can perform ASCII communication through any, or all, of its RS232 ports. The CoProc module does require BASIC programming to perform the ASCII communication.

  • adccommunitymod (AutomationDirect)

    Created Date: May 04,2010

    Created by: jwbaker3

    Look at the DCM for the 205, maybe use it and free up port 2 on the CPU. I need one on a project where we needed a operator interface on 485 and a marquee using ASCII, worked great.

    John

  • adccommunitymod (AutomationDirect)

    Created Date: May 04,2010

    Created by: milldrone

    KPrice, or Bernie,

    Isn't a common problem with ascii serial comms, the fact the scale sends the info before the PLC is ready? I had heard that the co-pro eliminates this problem.

10 of 20