adccommunitymod (AutomationDirect) asked a question.

Space around PLC

Created Date: October 27,2009

Created By: dieseltwitch

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I noticed that, in the DL05 & 06 Spec Sheet that there is a required 2 " & 1.5 " (respectively) perimeter for placing other components around, its this NEC code, UL code or just MFG recommended? Can I negate that and go closer if put in a fan or can i just negate that a little bit, right now I have about an inch of space around the PLC.


  • adccommunitymod (AutomationDirect)

    Created Date: October 27,2009

    Created by: Bob S BN

    I believe it is only for ambient air flow for cooling.

    While I know it's not the right thing to do, I have retrifitted some in place of other PLCs with less than ideal space, and haven't had any trouble...YET..., knock on wood...

    I imagine the space top to bottom would be more important than the sides.

    Just my $.02

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: October 27,2009

    Created by: KPrice

    dieseltwitch, well, it could be considered both NEC and UL code, and could be rejected upon inspection. While the NEC does not govern pre-built OEM control panels, the inspector could require either the panel to be built in a "listed " shop, or be inspected by a 3rd-party inspection agency. The "listed " shop or 3rd-party inspection would follow UL, and UL requires that the manufacturer's literature be followed in the installation and operation. The installation instructions is part of the component being UL listed.

    So, yes, in a long, 'round-about-way, it is "NEC code, UL code, and MFG recommendation ". Hope this saves you some hassle.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: October 28,2009

    Created by: Kristjan H

    The space is mostly about cooling.

    If you stuff the PLC in a tight place, you need to think of the PLC temperature. We have had some serious issues that we can't link to anything but heat buildup. The PLC was crammed in the cabinet and even though we had a ventilation fan on the cabinet it didn't provide much cooling. I measured over 50°C right above the PLC base and before long the analog modules started failing. We had more powerful ventilation installed to ensure cooling and right now the PLC temp is about 30-35°C. That makes a huge difference.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: October 29,2009

    Created by: dieseltwitch

    Thanks everyone thats what i was looking for.

  • adccommunitymod (AutomationDirect)

    Created Date: October 27,2009

    Created by: dieseltwitch

    I noticed that, in the DL05 & 06 Spec Sheet that there is a required 2 " & 1.5 " (respectively) perimeter for placing other components around, its this NEC code, UL code or just MFG recommended? Can I negate that and go closer if put in a fan or can i just negate that a little bit, right now I have about an inch of space around the PLC.