adccommunitymod (AutomationDirect) asked a question.
moving rungs between projects
Created Date: October 02,2009
Created By: c505ber
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Is there a way to copy or move rungs from one project to another?
Created Date: October 02,2009
Created by: bcarlton
With projects 1 (source) and 2 (target) open, project 2 in Edit Mode:
In project 1:
1. Click at left side of the desired rung
2. Press shift-down arrow to highlight
3. Continue to hold shift and press down arrow to select more contiguous rungs
4. Click Copy symbol or press CTRL-C
In project 2:
1. Click to the left side on rung above which you wish to insert the copied rungs
2. Press Paste symbol or press CTRL-V
3. Select the method of handling any labels and press Paste It.
Created Date: October 02,2009
Created by: KPrice
Yes, as bcarlton suggests. And to open the second project, open a second instance of DirectSOFT, by double-clicking on the DirectSOFT icon, for example. Then open the second project using this second instance of DirectSOFT.
Created Date: October 02,2009
Created by: franji1
The source project does not need to be in EDIT mode, but the destination project DOES need to be in EDIT mode
Created Date: October 02,2009
Created by: c505ber
Thanks
I was missing the having 2 instances of Dsoft open at the same time
Created Date: October 02,2009
Created by: c505ber
Is there a way to copy or move rungs from one project to another?