adccommunitymod (AutomationDirect) asked a question.

Losing Link name on power loss

Created Date: August 07,2009

Created By: toml

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I am using Lookout v5.1 and Lookout Direct Plus with ethernet modules in each of about 11 DL205 plc's (240,250-1, and 260). If we lose power on the pc running lookout and power back up, 2 of links that come up in DSLaunch v5.1 are not the same as before the power loss. Specifically, one of the links to a DL260 is now Address 4 instead of "Push_Split ". This link also shows plc type 240 instead of the 260. In another link the link name comes up fine, but the plc type comes up 240 instead of 250.


  • adccommunitymod (AutomationDirect)

    Created Date: August 07,2009

    Created by: toml

    I am using Lookout v5.1 and Lookout Direct Plus with ethernet modules in each of about 11 DL205 plc's (240,250-1, and 260). If we lose power on the pc running lookout and power back up, 2 of links that come up in DSLaunch v5.1 are not the same as before the power loss. Specifically, one of the links to a DL260 is now Address 4 instead of "Push_Split ". This link also shows plc type 240 instead of the 260.

    In another link the link name comes up fine, but the plc type comes up 240 instead of 250.

    Expand Post