adccommunitymod (AutomationDirect) asked a question.
Created Date: May 18,2009
Created By: worknhard9062
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Very little in the Help files about these two guys. This includes DirectSoft32 Version 4.0 Build 25 and DirectSoft 5 Version 5.3. Both versions Help files refer to "the following example " but there IS no following example. I'm envisioning something along the lines of a sub-level Master Control Relays, slaved off of something, but not sure. Help indicates it has something to do with the PLC inputs??? Anyone use these or know anything about them? They could be "real handy " for one of my applications IF their purpose and function is what I hope. Thanks in advance.
Created Date: May 18,2009
Created by: bcarlton
Grab the free online 305 CPU manual. it has the example.
Created Date: May 18,2009
Created by: worknhard9062
Very little in the Help files about these two guys. This includes DirectSoft32 Version 4.0 Build 25 and DirectSoft 5 Version 5.3. Both versions Help files refer to "the following example " but there IS no following example.
I'm envisioning something along the lines of a sub-level Master Control Relays, slaved off of something, but not sure. Help indicates it has something to do with the PLC inputs???
Anyone use these or know anything about them? They could be "real handy " for one of my applications IF their purpose and function is what I hope. Thanks in advance.