adccommunitymod (AutomationDirect) asked a question.
Conversion to PSI
Created Date: September 22,2008
Created By: rromanelli
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I am using a analog input F4-16AD to receive a value from a sensor. My sensor is a 4-20mA and the range is -1 to 40 kg. I need to obtain the signal in V4005, but in PSI . I am using the formula tha exists in manual but the value is not correct What I need to do to convert the value to sensor to Vmemory ?
Created Date: September 22,2008
Created by: KPrice
rromanelli, I need to know the units for your sensor range, but for example I will assume your sensor range is: 4-20mA for -1 kg/cm2 to 40 kg/cm2. I have a conversion factor of 14.22 psi per kg/cm2. So after conversion, your range in psi is: 4-20mA for -14.22 psi to 568.8 psi. This gives a full-scale span of: 583 psi for the 0 to 4095 raw data. Do you agree with all of this so far? If your sensor range is in other units, then this would be incorrect. (I must be assuming the wrong units because this range seems strange to me.)
Your offset or "zero " is -14.22 psi. How do you want to handle the negative value, an BCD with a sign relay? real number? BCD with an offset? There have been other posts that pointed out the advantages and disadvantages to each method.
Created Date: September 22,2008
Created by: rromanelli
Conversion to PSI
Yes, this is the sensor range !!!
In my program I used the instruction according the manual to convert the value :
-LDF X20
K12
-BCD
-LDF X34
K4
-OUTX V4000
After this I used this : D= (H-L)/4095 ; (568-(-14,2))/4095
LD V4000
MUL K582
DIV 4095
OUT V5000
Is this correct ? I am using V5000 to view the value in PSI
Created Date: September 22,2008
Created by: rromanelli
I am using a analog input F4-16AD to receive a value from a sensor. My sensor is a 4-20mA and the range is -1 to 40 kg.
I need to obtain the signal in V4005, but in PSI .
I am using the formula tha exists in manual but the value is not correct
What I need to do to convert the value to sensor to Vmemory ?