adccommunitymod (AutomationDirect) asked a question.

4-20ma transmitter

Created Date: August 31,2008

Created By: david222

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

This question may be off topic some but I have recieved excellent help from this site. I am using a dl05 and a c-more mini micro to learn on and for class. Is there any way (meter, etc) to first test 4-20ma transmitter circuits and second is it possible to use this meter??? in place of the pressure transmitter. Just trying to possibly kill two birds at once, trying not to buy a pressure transmitter and get a test meter at the same time. Thanks DT


  • adccommunitymod (AutomationDirect)

    Created Date: August 31,2008

    Created by: Do-more PE

    If you are looking for something a little more specialized, Extech makes a nice unit . It's quite a bit cheaper, but all it does is voltage and current simulation/reading unlike the Fluke which has a ton of bells and whistles.

    I have one of their older models and it works quite well.

  • adccommunitymod (AutomationDirect)

    Created Date: August 31,2008

    Created by: Tubecut

    I seem to recall that there was a way, using a 250 ohm resistor to change the 4-20mA to 1-5 VDC. That leads be think that with a variable output power supply, the 4-20mA could be used. Not sure if this is where the OP wants to go.:confused:

  • adccommunitymod (AutomationDirect)

    Created Date: August 31,2008

    Created by: Tom Jenkins

    You can make a simulator for loop powered 4-20 mA by using a resistor and a potentiometer in series. A 1 kOhm in series with a 5 kOhm pot should be sufficient. I don't recommend it for field troubleshooting, but is sure saves time and money when you are doing shop testing of a system with a lot of analog inputs.

  • adccommunitymod (AutomationDirect)

    Created Date: August 31,2008

    Created by: david222

    This question may be off topic some but I have recieved excellent help from this site.

    I am using a dl05 and a c-more mini micro to learn on and for class. Is there any way (meter, etc) to first test 4-20ma transmitter circuits and second is it possible to use this meter??? in place of the pressure transmitter. Just trying to possibly kill two birds at once, trying not to buy a pressure transmitter and get a test meter at the same time.

    Thanks

    DT

    Expand Post