adccommunitymod (AutomationDirect) asked a question.

encoder

Created Date: July 10,2008

Created By: kevin91172

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Years back I made a automatic bag maker/sealer with a DL05/6 " ez touch HMI and an existing red loin encoder counter that counts number of inches to make different sizes a bags and close s dry contacts to give me input signal to the PLC.I want to replace the red loin control and just use the PLC.What is a good encoder/ counter module I can purchase to start this project? I want to input inches I want in my existing EZ touch screen to do this.


  • adccommunitymod (AutomationDirect)

    Created Date: July 11,2008

    Created by: Rich19551

    If you are using the 05/06 just buy H0-CTRIO HIGH SPEED COUNTER INTERFACE MODULE for it and use the incoder to input the count into the module.

  • adccommunitymod (AutomationDirect)

    Created Date: July 13,2008

    Created by: elevmike

    If your project isn't very fast, you might not need the counter interface. X0-X1 can be configured as HSC inputs up to 5kh.

  • adccommunitymod (AutomationDirect)

    Created Date: July 17,2008

    Created by: stimpsonjcat

    True, but the CTRIO does the scaling right in the card setup...pretty slick IMHO.

  • adccommunitymod (AutomationDirect)

    Created Date: July 10,2008

    Created by: kevin91172

    Years back I made a automatic bag maker/sealer with a DL05/6 " ez touch HMI and an existing red loin encoder counter that counts number of inches to make different sizes a bags and close s dry contacts to give me input signal to the PLC.I want to replace the red loin control and just use the PLC.What is a good encoder/ counter module I can purchase to start this project? I want to input inches I want in my existing EZ touch screen to do this.

    Expand Post