adccommunitymod (AutomationDirect) asked a question.

DL06 power supply question

Created Date: May 15,2007

Created By: hilltop

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

can i use a external 24volt dc supply along with the dl06 supply and just tie the negetives together or would that mess up the unit, i need to get a input to the plc but the signals are off another supply


  • adccommunitymod (AutomationDirect)

    Created Date: May 15,2007

    Created by: bcarlton

    If the source of the other supply is not too far away then tie the negatives together. If you are tying the negative sides to frame ground then do it at only one point. If the source is from another machine then use it for isolated inputs or outputs.

  • adccommunitymod (AutomationDirect)

    Created Date: May 15,2007

    Created by: hilltop

    the other supply is in the same unit but if i use a positive off that supply and put it into the plc input nothing happens so i was woundering if i could tie the plc 24v neg and the supply 24v neg together.

  • adccommunitymod (AutomationDirect)

    Created Date: May 15,2007

    Created by: bcarlton

    If you are wiring to an input just make sure that the connection to the input common is from the supply which powers the input device. The 24 VDC power supply contacts provided on a 110VAC powered unit are isolated from the input commons unless you wire them together. Check the wiring diagrams in the manual carefully.

  • adccommunitymod (AutomationDirect)

    Created Date: May 15,2007

    Created by: hilltop

    can i use a external 24volt dc supply along with the dl06 supply and just tie the negetives together or would that mess up the unit, i need to get a input to the plc but the signals are off another supply