adccommunitymod (AutomationDirect) asked a question.

D2-260 Port 1 Status

Created Date: May 05,2007

Created By: jesawyers

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Are there port 1 status relays in a D2-260 CPU like there is for port 2 (SP116,SP117)? I 've looked through all the documentation and didn't see anything. Thanks...John


  • adccommunitymod (AutomationDirect)

    Created Date: May 05,2007

    Created by: bcarlton

    Since Port 1 can't be used as a Master for any protocol there's little that the user program would be able to do with it. The program can't initiate any communications nor can it control (directly) the responses. Hence (I guess) no status relays are available for thye user program.

  • adccommunitymod (AutomationDirect)

    Created Date: May 05,2007

    Created by: milldrone

    jesawyers,

    The only one I could find (in an 06)is sp46 "comunications error " on when a comunication error occurson any of the communication ports

  • adccommunitymod (AutomationDirect)

    Created Date: May 05,2007

    Created by: jesawyers

    Are there port 1 status relays in a D2-260 CPU like there is for port 2 (SP116,SP117)? I 've looked through all the documentation and didn't see anything.

    Thanks...John