adccommunitymod (AutomationDirect) asked a question.
Created Date: November 19,2006
Created By: CLW@CrownCork
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Hello everyone, My first post here. I was writing small programs to help train a new employee. The objective was to see how many ways we could toggle a single output, with a single input. In the following example, I used a shift register to shift a bit through the word, and had it do different pulses when on each time. No problem. The weird thing is that the output would not respond (energize) if I only used the particular register bit that was on at the time (C10, C12, C14, C16) in the line of code for the Y0 output. I had to use another relay(C2) as the "on " bit for the output Y0. Does anyone know why this is? I felt a bit silly when I was trying to show him something, and it didn't work at first. I told him I didn't quite understand why it didn't work without the additional relay, and would give it more thought. Well, I did, and I still don't know. Anyone see the obvious thing I must be overlooking to help descramble my brain? PLC 05 // Rung 1 // Address 0 STRN X0 ANDN C2 ANDN C10 ANDN C11 ANDN C12 ANDN C13 ANDN C14 ANDN C15 ANDN C16 SET C0 // Rung 2 // Address 10 STR C1 RST C0 // Rung 3 // Address 12 STR X0 OUT C1 // Rung 4 // Address 14 STR C0 STR C1 STR C17 SR C10 C17 // Rung 5 // Address 19 STR C10 OR C12 OR C14 OR C16 OUT C2 // Rung 6 // Address 24 STR C2 AND C10 STR C2 AND C12 AND SP4 ORSTR STR C2 AND C14 AND SP5 ORSTR STR C2 AND C16 AND SP6 ORSTR OUT Y0 // Rung 7 // Address 39 END #BEGIN ELEMENT_DOC "X0 ", "PROX X0 ", " ", "Sensor " "Y0 ", " ", " ", "Light " "C0 ", " ", " ", "SR Data Entry Bit " "C1 ", " ", " ", "SR Clock Pulse Bit " "C2 ", " ", " ", "Y0 " "On " " Bit " "C10 ", "SR BIT 0 ", " ", " " "C11 ", "SR BIT 1 ", " ", " " "C12 ", "SR BIT 2 ", " ", " " "C13 ", "SR BIT 3 ", " ", " " "C14 ", "SR BIT 4 ", " ", " " "C15 ", "SR BIT 5 ", " ", " " "C16 ", "SR BIT 6 ", " ", " " "C17 ", "SR BIT 7 ", " ", "SR Reset Bit " #END
Created Date: November 20,2006
Created by: crown spec pack
Heh, forgot my other password, and I can't get to my other email right now.
Anyone look at this at all? I guess it's not that important (doesn't equate to production downtime if I don't figure out why it doesn't work), but if someone knows right away looking at it, could you let me know? I just don't understand why it doesn't work without the additional C2 coil.
If no one replies I won't bug you again, promise. I'll assume I was right and it's not important/appropriate for the forum. No worries! The machines are all running http://forum1.automationdirect.com/board/smile.gif
Thanks!
Created Date: November 20,2006
Created by: bcarlton
I loaded it but could not see any reason why the outputs would not properly energise without the intermediate bit.
Created Date: November 21,2006
Created by: crown spec pack
Thanks bcarlton,
I appreciate your time. Thanks for checking it out. Oh well. Later http://forum1.automationdirect.com/board/smile.gif
Created Date: November 27,2006
Created by: researcher
Can you try something. I had something similar, maybe not quite the same but I added 'nop ' commands between outputs. I had 5 outputs that indicated different alarms. Individually they would work but if I purposely created the 5 alarms so that they would all come on at the same time, I would only get every other output on. I added 4 'nop ' commands between the code for each output and the alarms worked OK. This is weird but I experienced this. Maybe you can try this to see if it solves your problem.
Created Date: November 19,2006
Created by: CLW@CrownCork
Hello everyone,
My first post here. I was writing small programs to help train a new employee. The objective was to see how many ways we could toggle a single output, with a single input.
In the following example, I used a shift register to shift a bit through the word, and had it do different pulses when on each time. No problem.
The weird thing is that the output would not respond (energize) if I only used the particular register bit that was on at the time (C10, C12, C14, C16) in the line of code for the Y0 output. I had to use another relay(C2) as the "on " bit for the output Y0.
Does anyone know why this is? I felt a bit silly when I was trying to show him something, and it didn't work at first. I told him I didn't quite understand why it didn't work without the additional relay, and would give it more thought.
Well, I did, and I still don't know. Anyone see the obvious thing I must be overlooking to help descramble my brain?
PLC 05
// Rung 1
// Address 0
STRN X0
ANDN C2
ANDN C10
ANDN C11
ANDN C12
ANDN C13
ANDN C14
ANDN C15
ANDN C16
SET C0
// Rung 2
// Address 10
STR C1
RST C0
// Rung 3
// Address 12
STR X0
OUT C1
// Rung 4
// Address 14
STR C0
STR C1
STR C17
SR C10 C17
// Rung 5
// Address 19
STR C10
OR C12
OR C14
OR C16
OUT C2
// Rung 6
// Address 24
STR C2
AND C10
STR C2
AND C12
AND SP4
ORSTR
STR C2
AND C14
AND SP5
ORSTR
STR C2
AND C16
AND SP6
ORSTR
OUT Y0
// Rung 7
// Address 39
END
#BEGIN ELEMENT_DOC
"X0 ", "PROX X0 ", " ", "Sensor "
"Y0 ", " ", " ", "Light "
"C0 ", " ", " ", "SR Data Entry Bit "
"C1 ", " ", " ", "SR Clock Pulse Bit "
"C2 ", " ", " ", "Y0 " "On " " Bit "
"C10 ", "SR BIT 0 ", " ", " "
"C11 ", "SR BIT 1 ", " ", " "
"C12 ", "SR BIT 2 ", " ", " "
"C13 ", "SR BIT 3 ", " ", " "
"C14 ", "SR BIT 4 ", " ", " "
"C15 ", "SR BIT 5 ", " ", " "
"C16 ", "SR BIT 6 ", " ", " "
"C17 ", "SR BIT 7 ", " ", "SR Reset Bit "
#END