adccommunitymod (AutomationDirect) asked a question.
Created Date: September 12,2006
Created By: trevorstripling
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I have downloaded and got the calc RPM example working for my application, but the input sensor I have only pulses 4 times per revolution and does not give me enough resolution at low rpms. I have a shaft that starts at 0 rpm and ramps up to 8000. I need to sample 100-200 times per second to ensure it is not increasing in speed faster than a predetermined acceleration rate. What I need to do (or at least think) is instead of count the pulses per time period to determine the shaft rpm, is to trap the amount of time between pulses instead. Can anyone give me a good example of how to do this with a DL06 using the high speed inputs? Trevor
Created Date: September 26,2006
Created by: al.kaufman
I 've had to do the same recently on a PC based control system, but the logic is the same.
Use a 1-Shot on an immediate input of your pulse. Use the 1-Shot to grab the accumulated value of a timer. Divide 4000 by the accumulated value in milli-seconds to get the RPM, assuming 4 pulses per rev. Also put the 1-Shot as an N.C. contact as the condition to run / reset the timer. That's it.
Adjust the dividend according to the number of pulses per rev and resolution of your timer. ie: Use 600 for six pulses per rev and .01 sec ticks, etc.
Created Date: September 26,2006
Created by: Rich1955
Sp8------------udc 176
spo Nc---------udc 176
X3 incoderx4---udc 176
K9999999
X3 NC-----------Ld cta 176
out v2000
That is the fastest way I know
Created Date: September 26,2006
Created by: Rich1955
Sorry ment X2
Created Date: September 28,2006
Created by: twbrock
Sorry I took so long to get this posted by I have been busy. This works from 1 rpm to 1000 rpm and more as long as the scan rate is less than 60 mS. Only need 1 pulse per rev. Theta can be 1 to 99 but I am using 90 on a couple of units and this seams to work very well.
Rung 1
STR SP0
LD K6000
OUT V2104
LD K90
OUT V2105
LD K100
OUT V2106
Rung 2
STR X0
PD C0
Rung 3
STR C0
ANDN C1
STR C1
ANDN C0
ORSTR
OUT C1
Rung 4
STR C1
AND X1
STR C5
TMRAF T0 K30000
Rung 5
STRN C1
AND X1
STR C6
TMRAF T2 K30000
Rung 6
STRN C1
PD C3
Rung 7
STR C3
LD V2104
DIV TA0
OUT V2100
OUT C5
Rung 8
STR C3
MATHBCD V2102 "(V2102 * V2105) + ((V2106 - V2105) * V2100) "
DIV V2106
OUT V2102
OUT V2103
Rung 9
STR C1
PD C4
Rung 10
STR C4
LD V2104
DIV TA2
OUT V2101
OUT C6
Rung 11
STR C4
MATHBCD V2102 "(V2102 * V2105) + ((V2106 - V2105) * V2101) "
DIV V2106
OUT V2102
OUT V2103
Rung 12
STRN X1
LD K0
OUT V2100
OUT V2101
OUT V2102
OUT V2103
Rung 13
END
Created Date: September 28,2006
Created by: al.kaufman
Originally posted by al.kaufman:
I 've had to do the same recently on a PC based control system, but the logic is the same.
Use a 1-Shot on an immediate input of your pulse. Use the 1-Shot to grab the accumulated value of a timer.
The general equation is:
Speed (rpm)=60/(n*t) where: n=pulses/rev
t=time between pulses (sec)
Example:
for n=4, t=.030 sec Speed=60/(4*.030)=500 rpm
Note: If you use a standard input for the pulses, you want 2+ scans per on-off pulse.
This sets the max speed you can reliably measure at:
Speed=60/(n*tmin) where tmin= 2*scan time
Example:
for n=15, and scan time =.037 sec
Speed (max) = 60/(15*2*.037) = 54 rpm
Above that speed you need faster inputs, a faster scan, or a high speed counter.
I am doing this with a PC based control system which gives very fast scan times.
A standard prox on a regular input is fast enough for the rpm range I need.
Created Date: October 02,2006
Created by: stimpsonjcat
FYI, this is a standard feature of the Hx-CTRIO card. No code necessary.
Created Date: September 12,2006
Created by: trevorstripling
I have downloaded and got the calc RPM example working for my application, but the input sensor I have only pulses 4 times per revolution and does not give me enough resolution at low rpms. I have a shaft that starts at 0 rpm and ramps up to 8000. I need to sample 100-200 times per second to ensure it is not increasing in speed faster than a predetermined acceleration rate.
What I need to do (or at least think) is instead of count the pulses per time period to determine the shaft rpm, is to trap the amount of time between pulses instead.
Can anyone give me a good example of how to do this with a DL06 using the high speed inputs?
Trevor