adccommunitymod (AutomationDirect) asked a question.

Need cost effective way to measure angle of rotation

Created Date: July 18,2006

Created By: tubularfab

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I am looking for the most cost effective module and rotary encoder to measure the angle of a shaft that turns about 200 degrees max for a DL240 system. This is for monitoring a spindle on a mandrel tubing bender and I would like to have a resolution of at least .25 degrees - if not .1 degrees. Will the "D2-CTRINT " do it, or do I have to go to a "H2-CTRIO "? The spindle does not move very quickly - maximum I'm guessing is around 200 RPM. I do need a way for it to tell direction as well. Thank you, Jason


  • adccommunitymod (AutomationDirect)

    Created Date: July 18,2006

    Created by: Tech Guy

    Either module could possibly do it. The H2-CTRIO is a bit easier to setup, IMHO.

  • adccommunitymod (AutomationDirect)

    Created Date: July 19,2006

    Created by: tubularfab

    Ok, I have been scanning through the manual for the D2-ctrint and it does look like it will do want I need. But, I now have another question. I was planning on getting a quadtrature encoder with 360 pulses per revolution and using 4X count mode so I could have a resolution of .25 degrees per count. In one footnote, however, I noticed this "* This feature will allow the counter to count 4 times more with the same encoder (250"1/260 only). " Does that mean 4X counting only works on 250 and 260 cpu's but not the 240?

    Thank you,

    Jason

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: July 19,2006

    Created by: Tech Guy

    That is what it means. The 4x mode is available on the D2-250-1 and D2-260 only.

    Please be aware as well that the D2-CTRINT must go in slot 0 of the PLC rack next to the CPU.

  • adccommunitymod (AutomationDirect)

    Created Date: July 18,2006

    Created by: tubularfab

    I am looking for the most cost effective module and rotary encoder to measure the angle of a shaft that turns about 200 degrees max for a DL240 system. This is for monitoring a spindle on a mandrel tubing bender and I would like to have a resolution of at least .25 degrees - if not .1 degrees. Will the "D2-CTRINT " do it, or do I have to go to a "H2-CTRIO "? The spindle does not move very quickly - maximum I'm guessing is around 200 RPM. I do need a way for it to tell direction as well.

    Thank you,

    Jason

    Expand Post