adccommunitymod (AutomationDirect) asked a question.
Print command on DL06
Created Date: January 31,2006
Created By: cjenkins
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I am printing on a thermal serial printer from comm 2. All is working well, but I need to format the data going to the print. Ex. V2005 contains my current PSI (ex. 100.2 psi) so in my PRINT command it contains "PSI: " V2005:B and I get PSI: 1002 now I know I can divide V2005 by 10 and get PSI: 100 but I need to print out PSI: 100.2 Can anyone help?
Created Date: January 31,2006
Created by: testone
Print
"PSI: " V2005:B ". " V2006:B
You will need two register. One with 100 and one with 2. Do some math to get the 100 put into V2005 and the decimal into V2006.
V2005 = 1002 / 10
V2006 = 1002 - ((1002 / 10) * 10)
Created Date: January 31,2006
Created by: franji1
It's a little more complicated than that because the formatting of numbers does not provide you with just a "2 ".
Your example would print out
PSI: 0100 . 0002
because BCDs display leading 0s.
I 've done this once before - let me see if I can find the code.
Created Date: January 31,2006
Created by: franji1
Here's the program, complete with my own PRINT statement for testing (it prints the value out every second - I hooked up Hyperterminal to verify that it worked).
I loaded 1234 BCD into V2005 to make sure the digits came out right. This program uses V1400 thru V1403 for the ASCII buffer - you may need to change those addresses in the program.
Note that the PRINT statement now does a print with V1402%5 (print as ASCII text, length 5) instead of dealing with the raw BCD values. It's extra work, but you get the data formatted exactly as you want it.
=================
PLC 05
// Rung 1
// Address 0
#BEGIN COMMENT
"Every scan convert the 4 digit BCD value in V2005 to an ascii string of the form "
" " "###.# " ". To do this, I must use V1400/V1401 to convert the BCD digits to their ASCII "
"equivalent. Then I use V1402/V1403 for the output of massaging the text to insert the "
"decimal point. "
" "
"Then in the PRINT statement, I use the ASCII text %length modifier on V1402 (the length "
"is 5) "
#END
LD K1
LDA O2005
HTA V1400
LDD V1400
LDD K21436587
SFLDGT
OUTD V1402
SHFR K24
OUT V1404
LDD V1402
ANDD Kffffff
ORD K2e000000
OUTD V1402
// Rung 2
// Address 18
STR SP4
PD C0
// Rung 3
// Address 20
STR C0
PRINT K2 " " "PSI: " " V1402%5 " "$N " " "
// Rung 4
// Address 33
END
Created Date: January 31,2006
Created by: franji1
One minor issue - it will still print out leading 0's, that is if the value is 10.2 it will print "010.2 "
You cannot just replace the 0's with a space because 10.2 would display as " 1 .2 "
I hope this is acceptable
Created Date: January 31,2006
Created by: franji1
Actually - you are using an 06, so you could use VPRINT and then PRINTV to eliminate the leading 0's. Let me know if you would like this solution instead.
Created Date: January 31,2006
Created by: testone
Then he could do my simple example and make v2006 * 1000 so it prints
PSI: 0100.2000
Then it would look like a super accurate pressure reading..... http://forum1.automationdirect.com/board/wink.gif
Created Date: February 01,2006
Created by: cjenkins
Thanks for the help. The leading zero's before the decimal point is fine, but not 100.2000 franji1, I would like to see your code, it may make my customer happier than 090.2 I thank all for the advice.
CJ
Created Date: February 01,2006
Created by: testone
Sorry, I have 1 more idea but it is bulkier....
User 10 Print statements...
V2005 = PSI / 10
V2006 = PSI - (V2005 * 10)
--- V2006 = 0 --- Print V2005:B ".0$N "
--- V2006 = 1 --- Print V2005:B ".1$N "
--- V2006 = 2 --- Print V2005:B ".2$N "
--- V2006 = 3 --- Print V2005:B ".3$N "
--- V2006 = 4 --- Print V2005:B ".4$N "
--- V2006 = 5 --- Print V2005:B ".5$N "
--- V2006 = 6 --- Print V2005:B ".6$N "
--- V2006 = 7 --- Print V2005:B ".7$N "
--- V2006 = 8 --- Print V2005:B ".8$N "
--- V2006 = 9 --- Print V2005:B ".9$N "
This would print leading zeros and single decimal... 0090.2 etc...
Created Date: February 01,2006
Created by: franji1
Originally posted by cjenkins:
Thanks for the help. The leading zero's before the decimal point is fine, but not 100.2000 franji1, I would like to see your code, it may make my customer happier than 090.2 I thank all for the advice.
CJ
Here it is, but I did NOT use VPRINT/PRINTV - I just used ladder logic to replace the leading 0's with spaces. Note that the resulting character buffer occupies 3 words, not 2 (I had it wrong in the comment - the program was correct still).
The output buffer is in V1402, V1403 AND V1404
Here it is:
=====================
PLC 05
// Rung 1
// Address 0
#BEGIN COMMENT
"Every scan convert the 4 digit BCD value in V2005 to an ascii string of the form "
" " "###.# " ". To do this, I must use V1400/V1401 to convert the BCD digits to their ASCII "
"equivalent. Then I use V1402/V1403/1404 for the output of massaging the text to insert "
"the decimal point. "
" "
"THIS IS 5 CHARACTERS, DO IT TAKES UP 3 V MEMORY LOCATIONS, NOT TWO "
"AS I ORIGINALLY HAD DOCUMENTED (but had programmed correctly) "
" "
"In the NEXT rung, massage the text data in the accumulator to display leading spaces "
"instead of leading 0's. "
" "
"Then in the PRINT statement, I use the ASCII text %length modifier on V1402 (the length "
"is 5) "
#END
STR SP1
LD K1
LDA O2005
HTA V1400
LDD V1400
LDD K21436587
SFLDGT
OUTD V1402
SHFR K24
OUT V1404
LDD V1402
ANDD Kffffff
ORD K2e000000
// Rung 2
// Address 18
#BEGIN COMMENT
"The ASCII text is in the accumulator in this form numerically (due to how ascii characters "
"are stored) "
" "
"Bits 31-24 - " ". " " "
"Bits 23-16 - UNITS DIGIT "
"Bits 15- 8 - TENS DIGIT "
"Bits 7- 0 - HUNDREDS DIGIT "
" "
"So if the original value is less than 1000, (e.g. 0999), we want to replace the leading zero "
"character with the space character (hex 20). Mask off the HUNDREDS DIGIT and "
"replace it with 20 hex. "
" "
"AND if the original value is less than 100 (e.g. 0099), we want to replace the 2nd leading "
"zero character with the space character. Mask off the TENS DIGIT and replace IT with "
"20 hex. "
" "
"No need to worry about the UNITS digit, since we want a leading 0 for the units digit (e.g. "
"we prefer to see 0001 displayed as " "0.1 " " not " ".1 " " "
#END
STRN V2005 K1000
ANDD Kffffff00
ORD K20
ANDN V2005 K100
ANDD Kffff00ff
ORD K2000
// Rung 3
// Address 30
#BEGIN COMMENT
"Now that we have the accumulator formatted correctly with the first 3 digits and the "
"decimal points, output it to V1402/V1403 "
#END
STR SP1
OUTD V1402
// Rung 4
// Address 32
STR SP4
PD C0
// Rung 5
// Address 34
STR C0
PRINT K2 " " "PSI: " " V1402%5 " "$N " " "
// Rung 6
// Address 47
#BEGIN COMMENT
"Test code - increments V2005 to test transitions from 9->10, 99->100, 999->1000 "
#END
STR C0
INC V2005
// Rung 7
// Address 50
END
Created Date: February 03,2006
Created by: cjenkins
Thanks for the help!