adccommunitymod (AutomationDirect) asked a question.

ECOM100 and Dataradio

Created Date: November 21,2005

Created By: dc

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

trying to use a DLO6, ECOM100 and DataRadio's wireless IP/Integra. I have the units working in "router " mode but the much simpler (and required) mode that I need is Bridge. I can get two PC's to ping accross the bridge but when I try PC to DL06, the replied ping from the ECOM100 comes back but times out due to an error in the reply. There are very few parameter changes that we can make to the radios. Has anyone had an experience similar to this? thanks


  • adccommunitymod (AutomationDirect)

    Created Date: November 22,2005

    Created by: GKiser

    dc,

    I have seen this before, but not with the particular equipment you are using. Currently every time I have run into this issue it ends up being fixed by a setting on the wireless device. So far each case I have seen is using different wireless devices, so I do not have a good feel as to what needs to change. All attempts in our lab to duplicate this problem have failed. We simply cannot make it happen.

    Since we cannot duplicate the "problem " (whether it is ours or the wireless device's configuration) it is very difficult to "fix. " We have thought about having the ECOM100 send out periodic gratuitous ARP requests to see if doing so might "teach " devices like your wireless how to contact it. This ARP request would simply be a telegram on the wire that "asks "... "Who has IP Address? Tell IP Address. " Where "IP Address " would be the ECOM100's own IP Address. So he is kinda like asking a rhetorical question that other devices on the network "hear. " All devices that hear that might "learn " where the ECOM100 is and how to contact it.

    If we decided to do this and produce a beta firmware for the ECOM100, would you be willing to give it a try as a beta site? (You can always revert back to your regular firmware).

    Greg Kiser

    Host Engineering, Inc.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: May 02,2008

    Created by: GKiser

    It has been a long time coming...

    After much troubleshooting, we were finally able to duplicate these types of very rare and mysterious errors and discovered some definite bugs in the ECOM100 / EBC100 firmware.

    We believe these mysterious problems are fixed in the latest firmware. Firmware is available for download via NetEdit Live Update:

    H0-ECOM100 v4.0.222

    H2-ECOM100 v4.0.1444

    H4-ECOM100 v4.0.1444

    H2-EBC100 v4.0.518

    T1H-EBC100 v4.0.1325

    Greg Kiser

    Host Engineering, Inc.

    support@hosteng.com

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: November 21,2005

    Created by: dc

    trying to use a DLO6, ECOM100 and DataRadio's wireless IP/Integra. I have the units working in "router " mode but the much simpler (and required) mode that I need is Bridge. I can get two PC's to ping accross the bridge but when I try PC to DL06, the replied ping from the ECOM100 comes back but times out due to an error in the reply. There are very few parameter changes that we can make to the radios. Has anyone had an experience similar to this? thanks

    Expand Post