adccommunitymod (AutomationDirect) asked a question.

addressing input card for D0-05

Created Date: October 13,2005

Created By: kuyken37

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I am programing a D0-05 and have an 8 input card in the slot but am having trouble with the addressing. It shows up when I go to the I/O config, what addresses do I need to use?


  • adccommunitymod (AutomationDirect)

    Created Date: October 13,2005

    Created by: marksji

    The inputs will start at X100 on a DL05 or DL06. X0-X777 are used/reserved for the built in I/O.

  • adccommunitymod (AutomationDirect)

    Created Date: October 13,2005

    Created by: kuyken37

    Thank you

  • adccommunitymod (AutomationDirect)

    Created Date: October 14,2005

    Created by: franji1

    kuyken37,

    I am very interested in what DirectSoft's I/O configuration showed for the addresses. We read this from the CPU and would like to know if it is correct or not (could be DSP problem OR CPU problem).

    Go to PLC->Configure I/O and tell me what addresses show up in the "Slot 1 Addr In " field.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: October 13,2005

    Created by: kuyken37

    I am programing a D0-05 and have an 8 input card in the slot but am having trouble with the addressing. It shows up when I go to the I/O config, what addresses do I need to use?