adccommunitymod (AutomationDirect) asked a question.
DL06 Port 2
Created Date: October 03,2005
Created By: WilTech
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Hello all, I would like to know how to setup port 2 of the DL06 via ladder (instead of using Directsoft). I see that v7655 and v7657 are used to set protocol, baud, etc.. The problem is I want to setup the port for "Non-Sequence " protocol to use ASCII in/out. Can this be done? In the help topics it only list K-sequence, DirectNet and Modbus. Thanks in advance. WilTech
Created Date: October 03,2005
Created by: Tech Guy
See this application note which will explain it. There are links on the right side of the page for non-sequence.
Created Date: October 03,2005
Created by: WilTech
Thanks Tech Guy,
That explains it.
WilTech
Created Date: October 04,2005
Created by: marksji
This may help some too. This is the setup I use to print to a serial printer with the DL06. The port settings end up as 9600-8-N-1
http://www.samjackson.com/ad/port2-setup.pdf
Created Date: October 03,2005
Created by: WilTech
Hello all,
I would like to know how to setup port 2 of the DL06 via ladder (instead of using Directsoft). I see that v7655 and v7657 are used to set protocol, baud, etc.. The problem is I want to setup the port for "Non-Sequence " protocol to use ASCII in/out. Can this be done? In the help topics it only list K-sequence, DirectNet and Modbus.
Thanks in advance.
WilTech