adccommunitymod (AutomationDirect) asked a question.
clarification on DL05 with digital outputs
Created Date: April 22,2004
Created By: mpiotro
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I have an application where I will use a DL05 Plc. My power supply is 12 Vdc. I don't know whether the D0-05DD is an option, as I am confused by 2 conflicting statements on the DC output specs: 1. output voltage range = 6-24V dc 2. external dc power required = 20-28V dc, 150mA max. Can I use my 12V dc supply with these outputs (sinking)? Can someone clarify this for me??
Created Date: April 22,2004
Created by: mpiotro
I have an application where I will use a DL05 Plc. My power supply is 12 Vdc. I don't know whether the D0-05DD is an option, as I am confused by 2 conflicting statements on the DC output specs:
1. output voltage range = 6-24V dc
2. external dc power required = 20-28V dc, 150mA max.
Can I use my 12V dc supply with these outputs (sinking)? Can someone clarify this for me??
Created Date: April 22,2004
Created by: JimHoward
Mpiotro,
In order for the outputs of the D0-05DD to function, it needs 24 VDC power to operate the transistor output of the internal opto-isolator.
With the 24 VDC power in place, the second stage of the output circuitry (another transistor) then switches your 6-27 VDC to the field device attached to the output screw terminal.
Look carefully at the diagram "internal module circuity " in the catalog or manual. You will see that both 24 VDC AND the other 6-27 VDC power supplies are required.
Thus, if 12 VDC is the only power you have, the outputs won't work! (If 12 VDC is the only power you have, what is powering the PLC CPU? http://forum1.automationdirect.com/board/smile.gif ).
Jim
Created Date: April 22,2004
Created by: marksji
Originally posted by JimHoward:
Mpiotro,
(If 12 VDC is the only power you have, what is powering the PLC CPU? http://forum1.automationdirect.com/board/smile.gif ).
Jim
The D0-05DD-D is 12/24VDC powered. The CPU runs just fine on 12VDC.
I know with the D0-05DR (also 12/24VDC powered) the relay outputs will activate just fine on 12VDC. I 've got on in my truck and it works great except when starting (the truck). The DL05 doesn't recover from brownout. A small 12v battery and diode solved that problem though.
Created Date: April 23,2004
Created by: mpiotro
Guys, thanks for your help. I'll go with the D0-05DR-D (12V/24V dc in, relay out).