adccommunitymod (AutomationDirect) asked a question.

Lookout Display Info.

Created Date: February 07,2004

Created By: sdsmith

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I have a customer that would like to be able to view which of the lights on his controller (which includes a serial remote controller, both 405 units 440 and RS)are lite. This includes not only the power/run/cpu/batt,i/o,com etc. on the Master, and the pwr,I/o, run, par,diag,link but also the lights on the relay output modules. I 've been able to make the diagram for the controllers on the Lookout page along with the lights, but for most of the lights are unable to show if they are active or not.... what I need is the location to display (V or whatever) so that I can activate the "lights " on the Lookout display. Thanks...


  • adccommunitymod (AutomationDirect)

    Created Date: February 07,2004

    Created by: sdsmith

    I have a customer that would like to be able to view which of the lights on his controller (which includes a serial remote controller, both 405 units 440 and RS)are lite. This includes not only the power/run/cpu/batt,i/o,com etc. on the Master, and the pwr,I/o, run, par,diag,link but also the lights on the relay output modules. I 've been able to make the diagram for the controllers on the Lookout page along with the lights, but for most of the lights are unable to show if they are active or not.... what I need is the location to display (V or whatever) so that I can activate the "lights " on the Lookout display. Thanks...

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: February 09,2004

    Created by: Tech Guy

    The "run " light is easy, use SP1. The "coms " LEDs would be impossible to simulate as the coms speed to Lookout just isn't fast enough. The "bat " light can be found at SP43. The Power and CPU lights are easy as well. If either of those are lit, Lookout will loose communications, so...

    As far as I know Lookout cannot access most of the diag data from the I/O cards, so that leaves them out.

    Most of this information can be found in appendix "D " of the user manuals.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: February 10,2004

    Created by: ericn

    As Tech Guy stated, creative use of the SP relays (in Appendix D) is going to be your best bet to display the PLC status. For the output lights, why not just use the bit map for the output status? V40500-V40577 contain the status of ALL the possible output points (See pages 3-43 and 3-44 in the 405 User Manual).

    -Eric

  • adccommunitymod (AutomationDirect)

    Created Date: February 10,2004

    Created by: sdsmith

    Thanks for the replies, I really apprec. it.

    Sean