adccommunitymod (AutomationDirect) asked a question.
Created Date: January 16,2004
Created By: franji1
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
DNLoader is a utility to help OEMs (or anyone else) who wants to do "field upgrade " of their PLC programs WITHOUT their end-customers to have DirectSoft (or to "protect " their intellectual property). It's on Host Engineering's website under "utilities ", or click on http://www.hosteng.com/SW-Products/SP_Demo_Utilites.htm#DNLoader Here's an excerpt from the README file: DNLoader is a free utility that allows you to upload and download PLC programs without the use of DirectSOFT. Use DNLoader to read the ladder program and (optionally) the retentive V-memory register values from a DirectLOGIC PLC and save this data in a file. You can then use DNLoader to write the contents of this file to another DirectLOGIC PLC of the same type. DNLoader can use either a serial connection or an Ethernet connection (via an ECOM) to communicate with the source and destination PLCs.
Created Date: January 16,2004
Created by: franji1
DNLoader is a utility to help OEMs (or anyone else) who wants to do "field upgrade " of their PLC programs WITHOUT their end-customers to have DirectSoft (or to "protect " their intellectual property).
It's on Host Engineering's website under "utilities ", or click on http://www.hosteng.com/SW-Products/SP_Demo_Utilites.htm#DNLoader
Here's an excerpt from the README file:
DNLoader is a free utility that allows you to upload and download PLC programs without the use of DirectSOFT.
Use DNLoader to read the ladder program and (optionally) the retentive V-memory register values from a DirectLOGIC PLC and save this data in a file. You can then use DNLoader to write the contents of this file to another DirectLOGIC PLC of the same type.
DNLoader can use either a serial connection or an Ethernet connection (via an ECOM) to communicate with the source and destination PLCs.
Created Date: January 16,2004
Created by: Rday
Could a customer also use this to upload the code from a PLC and then download it to several other PLC's in effect copying the original code?
Created Date: January 16,2004
Created by: franji1
Yup. That's its function. So if you had more of a "manufacturing " environment - you could streamline the "PLC programming " aspect of it using this utility.
It is a no-frills utility - it is NOT meant for debugging! Think of it as an PLC programmer's "firmware download " utility (equating the PLC programmer's ladder logic/user memory as "firmware " to his/her end-user)
Created Date: January 16,2004
Created by: timyoung
Rday, the program can still be protected by a password if that's a concern.
Created Date: January 19,2004
Created by: franji1
Thanks, Tim, I misunderstood his question. Basically if you password protect your PLCs out in the field, the OEM must enter the password on HIS side of the DNLoader function (the "suck it out " half, before he ships out the file). Then, when the end customer tries to use DNLoader to download it to the PLC, the password must work (the end-user does not enter the password, the software does it automatically, unknown by the end-user). If it does not work, the end-user gets a warning message.
Created Date: February 03,2004
Created by: cdobis
I can't seem to get this utility to "Write File. " I can read from the PLC just fine, but when attempting to save it to file, with or without the password, it gives me an, "An unknown error occurred while accessing C:\DirectSOFT4\Program\PLCFour.dat.
What am I doing wroing here? BTW, this is Win2K on an Athlon 1gig with 512K.
Thanks,
CD
Created Date: February 03,2004
Created by: cdobis
...one other thing I forgot to mention, all of my PLCs are on the network via Ecom modules, DL260s for CPUs, why did I have to hit the "Select " about a dozen times before it can see any of my PLCs on the network? The Serial hookup works fine, first time, but not the Ethernet. Any ideas?
Thanks,
CD
Created Date: February 03,2004
Created by: GKiser
cdobis, regarding the "An unknown error... " that was a bug in DNLoader. Just download the latest from our website (http://www.hosteng.com) and that problem should go away for you. As far as the multiple "Select " button thing . . . I'm checking on that one.
Greg Kiser
Host Engineering, Inc.
Created Date: February 04,2004
Created by: GKiser
cdobis, regarding the "Select " button thing . . . can you use NetEdit or NetEdit3 and see if you can see the ECOMs with it? For example, does it behave in a similar manner as the DNLoader?
Greg Kiser
Host Engineering, Inc.
Created Date: February 04,2004
Created by: cdobis
GKiser,
Thanks for the response. As for the multiple "Select " button presses, I have DL 'ed the NetEdit3, it finds the PLCs after about 13 presses. It seems to be worse than NetEdit. Could it be our network that causes that? Our IT dept. says it is the latest and greatest available.
As for DNLoader, the new versions works fine, except that it has trouble finding the PLCs also.
Thanks!