adccommunitymod (AutomationDirect) asked a question.
Created Date: August 27,2003
Created By: piscis
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Can anyone please email me an example of how to use the instruction SR "Shift Register? The 205 Manual is not very much help, I'm using the 250 and 260 CPU's. Any helpful documentation will be highly appreciated, White Papers, Tutorial, WebPage, anything on how to use the Shift Register. I have an 8 Stations Index Table and I need to Reject parts in Station 7 accoding to the Inspection outcome in Station 5. Thanks All anibal@telemetrika.com
Created Date: August 27,2003
Created by: piscis
Can anyone please email me an example of how to use the instruction SR "Shift Register?
The 205 Manual is not very much help, I'm using the 250 and 260 CPU's.
Any helpful documentation will be highly appreciated, White Papers, Tutorial, WebPage, anything on how to use the Shift Register.
I have an 8 Stations Index Table and I need to Reject parts in Station 7 accoding to the Inspection outcome in Station 5.
Thanks All
anibal@telemetrika.com
Created Date: August 28,2003
Created by: KPrice
piscis,
Here is an application that utilized the shift register instruction. A bottle-filling and capping machine continuously ejected bottles to a conveyor. A sensor detected if the cap was on correctly. The sensor output was the data input to the shift register. A photo eye detected the presence of the bottle The photo eye output was the clock input to the shift register. There was a reject arm that would reject a miscapped bottle. The reject arm was located at a given number of "bottle positions " (clock pulses) downstream from the sensor location. When the corresponding shift register relay turned on, it indicated that a faulty bottle was at the reject station, and the shift register relay energized an output to reject the bottle. Perhaps this instruction may be used for your index table.
Created Date: August 28,2003
Created by: ericn
It might help more if you first understand HOW a shift register works. Go here:
http://www.plcs.net/chapters/shift20.htm
Be sure to watch the animation as well!
-Eric
Created Date: September 02,2003
Created by: piscis
KPrice / ericn:
Thanks so much I now fully understand and can use Shift Register.
Thanks Again!!!!
Andy