adccommunitymod (AutomationDirect) asked a question.
Created Date: March 01,2003
Created By: tmiked
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I am using the DL06-DD and a F0-2AD2DA-2 reading one Analog Input( 0-5 V Pressure Transducer). If I calibrate it using my laptop everything works. If I switch to 'RUN ' mode nothing changes and everything works fine. BUT ! When I disconnect the serial RJ-45 connection, the pressure settings change by about 10%. I assume this is have some sort of ground problem (even though the laptop is ungrounded) But, I wondered if anyone had seen this exact or similar effect before.
Created Date: March 01,2003
Created by: tmiked
I am using the DL06-DD and a F0-2AD2DA-2 reading one Analog Input( 0-5 V Pressure Transducer). If I calibrate it using my laptop everything works. If I switch to 'RUN ' mode nothing changes and everything works fine. BUT ! When I disconnect the serial RJ-45 connection, the pressure settings change by about 10%. I assume this is have some sort of ground problem (even though the laptop is ungrounded) But, I wondered if anyone had seen this exact or similar effect before.