adccommunitymod (AutomationDirect) asked a question.

d05 with modem lost run mode

Created Date: February 28,2001

Created By: L 'FRED

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I use a do5 with a module D0-01MC real time clock an memory cartrige, connect with a modem USR sporter 14,4 (not S.I.)configured; 9600 1,8,none on port 2 For unknow reason, it lost run mode. I live the switch on run position an the green led "Run " stop lite. If a change run to stop or terminal mode nothings append,I power up the plc, to reaccess run mode. in August a change the plc for the same probleme a more (run stop and cpu light turn on). That type of fail append allways wend a try to connect by modem. What can I do to fix that trouble?


  • adccommunitymod (AutomationDirect)

    Created Date: February 28,2001

    Created by: L 'FRED

    I use a do5 with a module

    D0-01MC real time clock an memory cartrige, connect with a modem USR sporter 14,4 (not S.I.)configured; 9600 1,8,none on port 2

    For unknow reason, it lost run mode.

    I live the switch on run position an the green led "Run " stop lite. If a change run to stop or terminal mode nothings append,I power up the plc, to reaccess run mode.

    in August a change the plc for the same probleme a more (run stop and cpu light turn on). That type of fail append allways wend a try to connect by modem.

    What can I do to fix that trouble?

    Expand Post